Skip to main content

Kollmorgen Support Network

Wake and Shake Function WSCNFG 0 >

Wake and Shake Function WSCNFG 0 with S300, S400, S600, S700 Servostar drives

Wake and Shake Function WSCNFG 1 >

Wake and Shake Function WSCNFG 1 with S300 / S700 Servostar drives

Wake and Shake >

One of the basic functions in the drive of a brushless servomotor is the commutation. The commutation is the current transition of one winding of the motor to the next winding. Only in case of a correct commutation time respectively a correct…
Subscribe to Wake and Shake