Skip to main content

Kollmorgen Support Network

AKD Basic Position Move Using Modbus >

Modbus TCP is made easy in the AKD Basic drive with the use of "User Defined" Modbus registers.  These are the 5000 series Modbus address numbers.  The registers are defined in the Basic program and mapped to variables.  You can then…
Subscribe to user defined Modbus register