Skip to main content

Kollmorgen Support Network

S300 internal current resolution to trigger digital output mode 8 or 9 >

For the S300, what is the resolution of the trigger point to turn outputs on based on a < or > of actual current?  This would relate to I<actO1TRIG and I>actO1TRIG in O1MODE=8 or O1MODE=9. The internal current resolution is depends…
Subscribe to current resolution