Pular para o conteúdo principal

Test the Motion without Touching the Machine >

Designing and implementing a differentiated machine can be challenging, especially the motion portion. OEMs want optimum performance, but don't want to spend a lot of time with trial-and-error testing. High-performance motion means tight tolerances…

When Motion Matters - Kollmorgen Automation Suite™ makes the difference >

Machine builders have numerous choices when it comes to automation system solutions. Many of these solutions take advantage of standard specifications, such as IEC61131-e, to simplify the PLC programming required for machine control. Many automation…

Make Machine Building Faster and Easier with Kollmorgen Automation Suite™ >

Do you have to open multiple programs to develop, debug and deploy your automation application? Does the need to learn different programs and manage different data sets slow down your time to market? Does the need to find key information stored in…

Industry Leading Precision Velocity Control in Coating and Laminating Applications >

Web handling applications demand perfect velocity control - and rightly so, as anything less will result in unevenly applied coating across the substrate and an inferior, or even scrappable, product. What's at the heart of most velocity control…

Is Reducing Time to Market Important to Your Machine Design? >

September 10, 2010 - End users are taking longer in deciding to add or upgrade a machine and when the decision is made they want the machine delivered quickly. In such a highly competitive market, being able to deliver a machine in short order can be…

The Significance of Load to Motor Inertia Mismatch >

August 13, 2010- A servo system’s inertia ratio is a commonly misunderstood parameter. When dealing with stepper motors, articles and tutorials often instruct the control engineer to select a motor that will match the ratio as close to 1:1 as…

Direct Drive Technology Improves Flexo Printing Quality and Throughput >

July 15, 2010 - Flexographic printing technology has become increasingly popular because it more easily maintains printing quality and reduces startup time and waste. But flexo printing quality is dependent upon maintaining extremely accurate…

Integrated Model-Based Machine Design with Motion >

March 19, 2010 - Motion control applications are becoming increasingly challenging with higher performance, lower weight requirements, and increased functionality. Meeting these challenges often requires complex control algorithms, which call for…

Electro-Magnetic Interference Reduction Techniques >

February 17, 2010 - EMI (Electro-Magnetic Interference) comes in different forms, frequencies, and levels. Electronic equipment has different categories for both emissions and susceptibility. Under normal circumstances elimination is not possible so…

How Today's Flexible Digital Servo Drives Help OEMs Build a Better Machine, Faster >

February 17, 2010 - Advances in digital hardware technology and software innovations now allow for a single digital servo drive to be configured to work in a variety of machine control architectures. So what, you say? The advantage to the machine…