Salta al contenuto principale
Casi di successo | 2 minuti di lettura

COMPLETE MOTION SOLUTION FOR PACKAGING

Schleck enjoy the aromatic double

Intelligence and motion in the controller: How are new product ideas from innovative packaging machines

Three in one: the Italian packaging machine builders Lafer has an integrated drive and automation solution streamlines its duly cabinets. The company near Verona to date a combination of PLC, Motion Controller and servo amplifiers, Lafer uses today with the number of KOLLMORGEN AKD PDMM a device series, which provides all three functions under one roof.

The look in the cabinet of an earlier generation of machines makes compared to the current series the advantage of drive-based automation at a glance clear quickly. On the one hand, the separate control hangs next to the quite bulky acting motion controller, in turn controls the servo controller to the left placed. In contrast, the housing solution with the AKD PDMM devices from KOLLMORGEN has significantly slimmer. Less hardware, less cables, only the devices themselves are due to the integrated intelligent control a touch larger than the pure controller.Kollmorgen_Lollipop_PaoloFormilanLafer_EN “The KOLLMORGEN solution is much smarter, because it offers the same performance at a lower price,” says Paolo Formilan, sales manager at Lafer, the benefit together from the perspective of the machine builder. “We also save a lot of cabinet space and can also easily integrate other axes in the composite.”

 From product idea to the machine

 With the current development Lafer “Motion-02” an international food company currently packed two sweet lollipops in various flavors aroma protected in a double-bag. Was “Such a machine is still pending. Was the catalyst for the development – as so often in the packaging machinery - a new product idea including innovative packaging, “explains Paolo Formilan. The plant isolated at the beginning of the process through turning rotary boiler the lollipops in each 40 shots on the outside walls and fitted it with an adjacent conveyor pairs for the lollipop. A feed unit performs the confectionery into the packaging film tube, which is replaced immediately after its inner sealing seam. In a further step closes a synchronously clocked welding bar, the packaging film transversely to the direction of production. The separation of Doublepacks done according to the order stored in the control formulation in individual packs or longer strands for hygienic storage. Up to 550 Lollipops can be packaged per minute. 

Kollmorgen_Lollipop_torquemotors_ENFor programming of the complete sequencing of the Italian system integrator Logitronic from Carrè consistently uses in the region Vicenza mechatronic programming with the Pipe Network. The engineering tool belongs to the KOLLMORGEN Automation Suite and is the machine architecture from including the dependencies between the axes of an application in a very short time, clearly and accurately. User as Logitronic-owner Raffaele Cortese draw virtually the machine and program it at the same time. Instead of complex steps with the Pipe Network graphic descriptions come with drag-and-drop functions. Starting with a virtual master, all functions and relationships between components and all movements and define settings with graphical description blocks. In addition are the five standard IEC 61131-3 languages for control flow and PLCopen motion control function blocks for motion control.

Cam profile for smooth movements

From the perspective of the motion control out Lafer uses for flow wrapping machine mainly electronic cams. With these profiles, the company adapts the clocking perforation and sealing bar motions as to the continuous web speed, the tools always come in sync to the web speed is used. When servo controller for the perforation is additionally a separate register control via software module integrated. The data of a camera that detects a color bar, the controller reads directly. The packaging machine works with eight controllers, which in turn are two virtual master axes (electronic line shafts) in the composite. Therefore this application is a typical example of the benefits drive-based control systems and motion control represents Background: Especially with a mean number to be controlled axes - in the example Lafer in total eight - adult IPC solutions are priced usually too expensive. Who now but relies on a compact controller takes compromising machine performance into account because just at fast cycle packaging machines for the low-cost consumer goods market, the short cycle times are obtained from the scheme no longer sustainable. “We synchronize to a millisecond,” says Paolo Formilan. 

The control is possible in real time, because the integrated into the servo controller series AKD PDMM PLC and motion control is realized based on a proprietary controller with Power PC architecture. Thus, the devices are not subject to the constraints of limited processing resources.

Regulators collect data

The AKD Servo PDMM Logitronic also uses as a repository for signals. The standard inputs and outputs are consistently used in order to receive signals from sensors outside the actual movement and gather feedback to be processed directly in the drive PLC. On the cross-communication with EtherCAT, it is also immaterial, in which unit the bond accrues the data. “Wealth is not the number of interfaces in the drives out, we take the I / O system from KOLLMORGEN before the targeted expansion, without having to make costly changes to programming. That’s just the advantage of a scalable system, “said Raffaele Cortese.Kollmorgen_Lollipop_RaffaeleCortese_EN

Within this system - KOLLMORGEN Automation Suite - expanded the continuity and the choice of drive technology hardware. On the one hand allows the AKD PDMM combine servo controller with the pure servo amplifiers of the AKD and secondly this kit extends to the engine itself Means that machine builders and system integrators can freely choose whether to the servo controller with established synchronous and asynchronous servo motors connect and get additional individual tasks with linear or rotary direct drives. This rule freedoms create the basis to drive tasks can equip really perfect - without having to take on controller side constraints consideration must. In Lafer as synchronous servo motors operate from AKM simultaneously with KBM torque motors that drive the round tables to separate the Lollipops.

 

Kollmorgen_Lollipop_MotorGear_ENConclusion

Lafer The example shows the single high-performance products are not sufficient to compact packaging machines similar to automate slim. What is needed is an open space with solution components that are easily combined. “We also work with our system partners is becoming increasingly important. Here we work with KOLLMORGEN together for a long time, “says Raffaele Cortese. Packaging machinery manufacturers as Lafer may change because of the cooperation of system integrator and drive technology manufacturer much more intense focus on the development of new packaging concepts - and therefore bring machines to market faster.

 

Kollmorgen_Lollipop_FabioMassari_EN

 

 

 

 

 

 

About Kollmorgen

Kollmorgen is a leading provider of motion systems and components for machine builders around the globe, with over 70 years of motion control design and application expertise. Through world-class knowledge in motion, industry-leading quality and deep expertise in linking and integrating standard and custom products, Kollmorgen delivers breakthrough solutions unmatched in performance, reliability and ease-of-use, giving machine builders an irrefutable marketplace advantage.
Please contact us for more information.

Scarica come PDF

1G Motion System

Scopri il motion creato apposta per la tua macchina. 1G Motion System di Kollmorgen offre una gamma completa di opzioni e funzionalità per progettare senza compromessi.
Scopri di più

Guida introduttiva al dimensionamento e alla selezione di sistemi servo

When specifying servo motors, drives and cables, learn how to optimize motion by incorporating mechanical load, motion profile, ambient environment, cabling and other considerations into a system-wide approach.
Scopri di più

Progetta l'eccezionale

Kollmorgen crede nel potere del motion e dell'automazione per creare un mondo migliore.

Scopri di più

Altre Risorse

Subacqueo che fluttua nelle acque profonde dell'oceano, illustrando le condizioni estreme sottomarine rilevanti per la tecnologia dei motori per acque profonde.

Motion affidabile a 4.000 metri: IKM e Kollmorgen avanzano nel design dei motori per le profondità marine >

Scopri come IKM e Kollmorgen hanno co-progettato un sistema sottomarino di nuova generazione che opera in modo affidabile a profondità di 4.000 metri in condizioni estreme.
stabilimento produttivo con controllo del motion multiasse

Come ottimizzare il controllo del movimento motion multiasse nelle moderne celle di produzione >

Quando i sistemi di motion aumentano di scala, mantenere la sincronizzazione diventa sempre più difficile. Scopri come le moderne celle di produzione mantengono precisione, stabilità e produttività anche a velocità più elevate.

Cosmopack: la transizione strategica da sistemi specializzati a soluzioni di packaging flessibili >

Scopri come Cosmopack ha ottimizzato l'integrazione delle linee di confezionamento automatizzate grazie a un'architettura di motion decentralizzata, ottenendo soluzioni di packaging più flessibili.
Kollmorgen Automation Suite Brochure

Kollmorgen Automation Suite Brochure >

La piattaforma di riferimento per la programmazione dell'automazione macchina ad alte prestazioni, con motion e controllo pronti all'uso in pochi minuti.
Feedback ridondante del servomotore: quando il posizionamento a prova di guasto è indispensabile

Feedback ridondante del servomotore: quando il posizionamento a prova di guasto è indispensabile >

Nei dispositivi medici, nei sistemi di difesa e in molte applicazioni industriali, il guasto del sistema di motion non è un'opzione. Scopri come i servomotori con dispositivi di feedback integrati e ridondanti semplificano la sfida di assicurare la…

Guida introduttiva al dimensionamento e alla selezione di sistemi servo >

When specifying servo motors, drives and cables, learn how to optimize motion by incorporating mechanical load, motion profile, ambient environment, cabling and other considerations into a system-wide approach.

Veloce sviluppo di protesi ed esoscheletri di nuova generazione >

Humotech è stata fondata nel 2015 guidata da una semplice domanda: invece di costruire prototipi su prototipi, cosa accadrebbe se gli ingegneri potessero valutare la progettazione di protesi, ortesi, esoscheletri e altri concetti di macchine…

Un robot immergibile dal motion compatto ed efficiente per l'ispezione in servizio dei serbatoi di stoccaggio del carburante >

Kollmorgen ha aiutato molte aziende di diversi settori a incrementare le prestazioni, la qualità, la produttività e a ridurre i costi. Leggete qui i successi dei nostri partner.

Kollmorgen supporta Salvagnini nella costruzione di macchine per la lavorazione della lamiera, più efficienti dal punto di vista energetico >

Innovazione, competenza, servizio. In 60 anni di attività, questi tre impegni hanno permesso al Gruppo Salvagnini di raggiungere la leadership mondiale nel campo delle attrezzature per la lavorazione delle lamiere. Fornitore numero uno al mondo di…