Salta al contenuto principale

Kollmorgen Essentials™ Motion Systems Brochure >

Learn more about the new Kollmorgen Essentials Motion System — designed for value, ease, scale and performance.

DC7 Datasheet >

The DC7 motor controller family incorporates a combination of superior quality, flexibility, and efficiency for automated guided vehicle (AGV) and autonomous mobile robot (AMR) designers that only settle for the best.

AC7 Datasheet >

The AC7 motor controller family incorporates a combination of superior quality, flexibility, and efficiency for automated guided vehicle (AGV) and autonomous mobile robot (AMR) designers that only settle for the best.

Cirrus Datasheet >

Cirrus is a cloud-based solution, enabling efficient collaboration between employees on-site and at the office. It simplifies the commissioning work with tuning and verification of layouts. Cirrus includes both Cirrus Cloud and Cirrus Install.

System Manager NG Datasheet >

System Manager NG controls the whole vehicle system (NDC8) and its traffic flow. It handles transport orders, allocates vehicles, and selects routes for different transport assignments

U-Zone Datasheet >

A flexible solution to run customized applications in the vehicle controller

NDC 8 Visualizer Datasheet >

Visualizer is a user friendly web application that lets you supervise your NDC8 system in real time. Follow a live overview of the system and keep track of vehicle statuses - wherever you are. You can easily set up push notifications to get instant…

Direct Drive Linear Motors Brochure >

Kollmorgen offers direct drive linear motors to suit any application need. They’re fast, powerful, precise and maintenance-free. Our brochure has all the details.

PCMM2G Datasheet >

With up to 64 axes of synchronized motion control, the next-generation PCMM2G automation controller scales to take everything from simple machines to highly complex environments to the next generation of speed, performance and ease of use.

Tech Sheet: TBM2G Frameless Motors for Propulsion Systems and Extreme Environments >

Servo motors are often used in extreme environments — for example, submersible vehicle propulsion systems, spacecraft, semiconductor manufacturing under high-vacuum conditions, hygienic equipment subject to high-pressure washdowns, and more.

Tech Sheet: Embedding TBM2G Frameless Motors into Gimbal and Precision Actuator Systems >

A gimbal is a pivoting support that permits rotation of an object around an axis. Additional degrees of freedom can be obtained by combining or nesting two or more gimbals, with their axes of rotation at 90° apart.

Tech Sheet: Embedding TBM2G Frameless Motors into Compact Rotary Actuators >

An electric rotary actuator produces rotary motion to drive a load. In its simplest form, a direct drive motor is coupled directly to the load. Often, rotary actuators also incorporate a gearbox to increase torque while reducing speed. Appropriate…