Pular para o conteúdo principal

Tech Sheet: TBM2G Frameless Motors for Propulsion Systems and Extreme Environments >

Servo motors are often used in extreme environments — for example, submersible vehicle propulsion systems, spacecraft, semiconductor manufacturing under high-vacuum conditions, hygienic equipment subject to high-pressure washdowns, and more.

Tech Sheet: Embedding TBM2G Frameless Motors into Gimbal and Precision Actuator Systems >

A gimbal is a pivoting support that permits rotation of an object around an axis. Additional degrees of freedom can be obtained by combining or nesting two or more gimbals, with their axes of rotation at 90° apart.

Tech Sheet: Embedding TBM2G Frameless Motors into Compact Rotary Actuators >

An electric rotary actuator produces rotary motion to drive a load. In its simplest form, a direct drive motor is coupled directly to the load. Often, rotary actuators also incorporate a gearbox to increase torque while reducing speed. Appropriate…