Salta al contenuto principale

Kollmorgen Support Network

Questions & Answers

The below represents frequent questions our support, engineering and sales teams have been asked over the years. If you have a question, please submit our contact us form to reach our application engineering team.

I changed a parameter with the GUI and saved it to the EEPROM but after restarting the amplifier the old value was used. [ S300 ], [ S400 ], [ S600 ], [ S700 ]

Parameters may be changed via a fieldbus (during the initialization) or by a defined command sequence via the digital inputs (INxMODE 30).

Which settings are required for operating an induction machine? [ S300 ], [ S400 ], [ S600 ], [ S700 ]
What does Hardware Revision mean on the nameplate of the servo amplifier? [ S300 ], [ S400 ], [ S600 ], [ S700 ]

The Hardware Revision defines the development status of the servo amplifier. The same number can be found on the cover page of the instructions manual. Refer to page Hardware Revision Number.

What do I have to consider when using a residual current protective device (RCD) in a servo system? [ S300 ], [ S400 ], [ S600 ], [ S700 ]
Is it possible to use motors with a feedback system without commutation information as a primary feedback. [ S300 ], [ S400 ], [ S600 ], [ S700 ]

Yes. A Wake & Shake function determines the absolute position of the permanent Magnets in relationship to the stator windings. See page Wake and Shake.

What do the parameters on screen page U/F control mean? [ S300 ], [ S700 ]

The parameters are used to setup an induction machine without feedback (sensorless).

See pages Sensorless Control for Induction Machines (S300, S700) and Operating Induction Machines (S300-S700).

Is it possible to suppress the motor cogging? [ S300 ], [ S700 ]

Yes, but with S300 and S700 only. See page Cogging Suppression

What does Gray Code mean? [ S300 ], [ S400 ], [ S600 ], [ S700 ]

See the page GrayCode

Is full output current possible with S300 in single phase operation? [ S300 ]

See the page Single Phase Operation

Which motion task profiles are pre-defined? [ S300 ], [ S700 ]
How can I calculate the brake power? [ S300 ], [ S400 ], [ S600 ], [ S700 ]
Welche Firmen bieten Lichtleiter für SERCOS an?

z.B. Lapp und Honeywell

Welche PROFIBUS Karte passt in welchen Verstärker?
S600 Aufdruck auf der Frontplatte "PROFIBUS"
S300/S700/S600 Aufdruck auf der Frontplatte "PROFIBUS DP"
Was bedeutet folgende Twin-CAT-Diagnosemeldung beim Betrieb eines S300/700 über CAN:BoxState: SDO data mismatch at StartUp SDO-Upload-Fehler 0x 1800, SI 1: erwarteter Wert: 0x181, empfangener Wert: 0x40000181

Ab Firmware 2.51 wurde das Verhalten bzgl. der COB-ID an die CAN-Norm angepasst.

Solange TwinCAT nicht angepasst wird, kann beim S300/700 das alte Verhalten durch Setzen von BUSP1=1 wiederhergestellt werden.

Was muss ich bei der Hardwarekonfiguration des PROFIBUS-Verstärkers in der SPS beachten?

Zunächst muß die GSD-Datei importiert werden (koll045d.gsd). Dann bietet Ihnen die Steuerung den Verstärker als SR6xx an. Sie müssen die 4AX und die 6AX konfigurieren.

Die E-Adressen und A-Adressen müssen jeweils gleich sein.

Die Adressen der 6AX müssen direkt auf die Adressen der 4AX folgen.

Bei den „Eigenschaften –DP-Slave“ sollte die Ansprechüberwachung aktiviert sein.

Beachten Sie auch die Hinweise im PROFIBUS Handbuch.

Was für PROFIBUS Einstellungen kann/ muss ich am Verstärker vornehmen?

Einzig nötige und mögliche Einstellung ist die Adresse.

  • S600: unter „Basiseinstellungen“
  • S300/S700: unter „CAN-/ Feldbuseinstellungen“.

Die Baudrate ermittelt der PB-Chip automatisch. Sie kann nicht eingestellt werden.

Besonderheit bei S400: Wenn die Feldbusadresse (ADDRFB) Null ist, wird der Antrieb über die allgemeine (vom S400 Mastergerät vorgegebene) Adresse angesprochen.

Ich habe die PROFIBUS Adresse richtig eingestellt, aber der Antrieb meldet immer "n04" (Watchdog) bzw. reagiert nicht auf die Kommandos von der Steuerung. Was kann noch falsch sein?

1) Öffnen Sie in der Inbetriebnahme Software die Seite "PROFIBUS". Dort gibt es eine Anzeige der Baudrate. Steht diese fest auf dem in der Steuerung eingestellten Wert?

Nein => Überprüfen Sie die Busverdrahtung. Der Verstärker hat noch nicht einmal die Baudrate ermittelt, d.h. es findet selbst auf unterster Ebene noch keine Kommunikation statt. Weiterer Hinweis hierfür: Die Steuerungs-CPU meldet Stationsausfall.

Ja => weiter zu 2)

2) Auf der Seite "PROFIBUS" gibt es eine Zeile Input und eine Zeile Output bzw. Eingang und Ausgang (S300 / S700). Sind in den Zeilen Zahlen zu sehen oder nur „yyyy“?

Nur „yyyy“

=> Überprüfen Sie die Hardwarekonfiguration in Ihrer Steuerung (s.o.). Der Antrieb empfängt möglicherweise noch keine Daten. Ist in der Hardwarekonfiguration des Profibus die Ansprechüberwachung für die DP-Slaves aktiviert?

Es sind Zahlen zu sehen => weiter zu 3)

3) Eingang/ Ausgang bzw. Input/ Output sind immer auf die Steuerung bezogen, d.h. in der Zeile Ausgang stehen Daten, die von der Steuerung zum Regler gesendet werden. Was steht in der Zeile Eingang (Input) im PZD5?

Nur Nullen

=> Ist das Software- Enable über den Bus gesetzt? Am FB10 ist das der Eingang SW_Enable.

Ja, es sind trotzdem nur Nullen zu sehen.

=> Die Kommunikation funktioniert, aber der Antrieb wurde noch nicht initialisiert, d.h. die Profibusbetriebsart noch nicht eingestellt. Mit dem FB10 muss die Betriebsart im NutzDB eingetragen (meistens 2 für Positionieren) und der Eingang Init_Drive? gesetzt werden.

Verschiedene Zahlen ungleich Null. Weiter zu => 4)

4) In der Zeile Eingang wird im PZD3 und PZD4 die aktuelle Position übertragen. Aufgrund der hohen Auflösung (20 Bit pro Motorumdrehung) flackern die letzten Bits dieser Anzeige fast immer. Sehen Sie, daß sich im PZD4 die letzte Ziffer ständig ändert?

Nein, die Zahlen dort sind völlig unveränderlich (meistens bei Null).

=> Die Kommunikation funktioniert, aber der Antrieb wurde noch nicht initialisiert, d.h. die Profibusbetriebsart noch nicht eingestellt. Mit dem FB10 muss die Betriebsart im NutzDB eingetragen (meistens 2 für Positionieren) und der Eingang Init_Drive? gesetzt werden.

Ja, die letzte Ziffer im PZD4 springt ständig

=> Die Kommunikation funktioniert, die Profibusbetriebsart ist eingestellt, und die Prozessdaten werden übertragen. Jetzt müssen Sie in in die Details des STW und der verschiedenen PZD einsteigen.

Wie können in einem PROFIBUS System Fahraufträge synchron gestartet werden?

Um mehrere Antriebe synchron zu starten, kann es daher sinnvoll sein, die Fahraufträge über den Bus nur vorzubereiten und über einen digitalen Eingang zu starten. Siehe hierzu Seite Start von Fahraufträgen bei PROFIBUS Betrieb.

Wie sende ich einen Drehzahl - Sollwert über einen Feldbus?
Können S300/S400/S600 und S700 in einem SERCOS-Ring kombiniert werden?

Ja, ohne Einschränkung.