Salta al contenuto principale

Kollmorgen Support Network

Safe Handling of Linear Motors Technical Note

This technical note discusses the safety notes required due to the permanent magnets installed in the secondary parts of the linear motors. Observe these notes strictly. As a result of the high-energy magnetic fields as well as the associated high ferromagnetic forces of attraction, there can be a direct danger to health or indirect danger.

File Versions

Safe Handling of Linear Motors.pdf (19.1 KB)
–

This technical note discusses the safety notes required due to the permanent magnets installed in the secondary parts of the linear motors. Observe these notes strictly. As a result of the high-energy magnetic fields as well as the associated high ferromagnetic forces of attraction, there can be a direct danger to health or indirect danger.

About this Download

Taxonomy: