Salta al contenuto principale

Kollmorgen Support Network

Floating Point Conversion

Floating Point Conversion - htm files for calculating IEEE-754 - 32bit Hex to Floating-Point, and Floating-Point to Hex - This is useful for calculations involved in the Modbus RTU communications on the S200-CNS servo drive and the P7000 stepper drive.

File Versions

IEEE-754 Floating-Point Conversion.zip (18.12 KB)
–

Floating Point Conversion - htm files for calculating IEEE-754 - 32bit Hex to Floating-Point, and Floating-Point to Hex - This is useful for calculations involved in the Modbus RTU communications on the S200-CNS servo drive and the P7000 stepper drive.

About this Download