Skip to main content
blog | How do I know if my motor is explosion proof? |
|
2 minute read

When a spark ignites volatile gas inside a motor, an explosion proof design contains the internal combustion to prevent a greater explosion or fire.  An explosion proof motor is clearly marked with a nameplate that identifies its suitability for a given hazardous environment. 

Depending on the agency certifying the motor, the nameplate will clearly indicate the hazardous location Class, Division, and Group for which the motor is suited. The agencies that can certify motors for hazardous duty are UL (United States), ATEX (European Union), and CCC (China).  These agencies separate hazardous environments into Class - which defines the hazards that may be present in the environment; Division - which identifies the likelihood of the hazard being present under normal operating conditions; and Group - which identifies the specific materials present.

The UL criteria recognizes three classes of hazards: Flammable gases, vapors or liquids (Class I), combustible dusts (Class II), or ignitable fibers (Class III).  Division 1 indicates that hazardous materials are present under normal operating conditions, while Division 2 indicates materials are not likely present under normal conditions.  Group will specifically identify the hazardous material present, such as the common Class I materials of Acetylene (A), Hydrogen (B), Ethylene (C), or Propane (D).

The European Union has similar certification requirements that group the environments into zones.  Zones 0, 1, and 2 are designated for gas and vapors, while zones 20, 21, and 22 are designated for dust and fiber. The zone number designates the probability of the material being present during normal operation with zone 0 and 20 at very high, 1 and 21 at high and normal, and 2 and 22 at low.

As of October 2020, China requires motors that operate in hazardous environments to have CCC certification.  To obtain certification, the product is tested by a certified testing organization to the specific requirements designated by the Chinese government.

It is important to check the motor nameplate for the specific requirements, hazards present, and other environmental considerations to determine the explosion proof motor fit.  The explosion proof designation indicates the types of hazards that suit that specific motor.  Using an explosion proof motor in a hazardous environment in which it is not specifically rated can be dangerous.

Consult an Expert

Explosion Proof Motors

Explosion-proof versions of motors are designed to minimize the risk of explosion, and to contain any internal  explosion that may occur without allowing it to propagate to the outside environment.

Learn More

Engineer the Exceptional

Learn how to engineer exceptional machines, robots and vehicles with the highest-performing, most reliable motors, drives, automation solutions and more.

Learn More

Related Resources

Why use explosion proof motors? >

Electric motors generate heat under normal operating conditions and have the potential to generate a spark if a motor coil fails. Excessive motor case temperatures or a spark that is not properly contained can cause an explosion or ignite a fire in…