Skip to main content
blog | Reducing Defects while Improving ROI in Metal Stamping with Direct-Drive Technology |
|
2 minute read


Compared to mechanical and hydraulic presses, mechanical servo metal stamping presses use high torque brushless motors to create more complicated stampings at faster speeds. But the type of motors used—a traditional geared or chain drive system or a direct drive motor—can dramatically impact the final product. 

Modern stamping machines are highly sophisticated devices and can be quite expensive. They give fabricators the ability to create precise, often complex forms while meeting the need for high throughput and production. But that high throughput and production can pose a challenge: a higher production volume means it’s more difficult to inspect every piece and spot defects. 

For rough parts such as metal cups and cans or automotive parts, the finish on the product is secondary to its function. But for finished parts such as decorative metal trim on cookstoves or dishwashers, such as control panels or door covers, the stamping machine needs to produce products free from any errors. 

In a progressive feeding system, the mechanical limitations of a traditional motor and gearbox system create vibration, which impacts the final finish on the product. Traditional application uses oversized servos and gearbox to match inertia of large rolls. This system is also costly to maintain, limits index times and throughput, has a lower power density, and is less accurate. Using a direct-drive motor in next-generation stamping machines can increase speed and stroke optimization while requiring fewer parts and producing much less vibration throughout the process.
 

Fewer Parts, Less Vibration with Direct Drive

Direct-drive motors allow machine builders to use smaller motors with a high-resolution feedback design that couples directly to the load. This eliminates the need for mechanical transmission, such as the use of a gearbox, which is the area that typically introduces vibration into the production process. This creates a quiet and dynamic operation with a very long system lifetime. 

A direct-drive motor is also able to protect the system against excessive reaction torque and reduce system inertia by removing the gearbox and other related transmission elements. When creating finished-good stamping parts, this again helps to minimize vibration and disruption that could cause imperfections and allow for faster production. 
 

Fewer Parts, Improved Performance

Reducing vibration in the stamping process is the principal benefit when selecting a direct-drive motor, but there are other complementary advantages compared to a traditional rotary servo motor: reliability, size, power, speed and ROI. 

It’s a simple equation: fewer parts = higher reliability

Eliminating the gears, pulleys, seals, bearings and other components means that there are fewer parts to maintain and repair. Directly coupling to the load also improves positional, speed and dynamic accuracy. There is no hysteresis, backlash or lost motion in any direction. Any tuning or maintenance to correct for this in a standard mechanical transmission system is eliminated, making it less costly to maintain and repair over time. 

Smaller Motor, Same Power

However, a smaller motor doesn’t mean less power. A direct-drive cartridge  motor can provide up to 510 Nm of continuous torque with speeds up to 2500 RPM and overall power of 11,700 watts.  This can meet the needs of most medium speed and high torque applications, sometimes providing up to 50% more torque density than conventional servo motors. It also dramatically increases the power density of the system. With fewer components, the motor delivers as much power in a reduced size, allowing for a smaller overall machine. 

The power and related torque density of direct-drive cartridge motors allows them to achieve higher accelerations compared to similar servo motors. Coupled with the lack of vibration with the removal of the transmission system, this significantly reduces index times and increases throughput because the machines can produce more with less worry about defects. 

Reduced maintenance, more power, better throughput, less unscheduled downtime—all of these add up to significantly enhance the profitability of an application. Direct-drive technology allows for a longer usable life with fewer defects and greater production. There are fewer parts to install and maintain, lowering labor and parts cost for a lower cost, and time-intensive, machine. Compared to other types of motors, there is simply a greater ROI for direct-drive motors in metal stamping machines. 

Ready to take the next step and learn which direct-drive motion technology is right for your system? Contact one of our motion experts to see what we can do for you. 
 

Consult an Expert

Cartridge DDR®

Our exclusive Cartridge DDR® servomotors combine the performance advantages of a frameless motor with the ease of installation of a full-frame motor. The advanced electromagnetic design provides up to 50 percent more torque density than comparably sized conventional servo motors.

Learn More

Engineer the Exceptional

Learn how to engineer exceptional machines, robots and vehicles with the highest-performing, most reliable motors, drives, automation solutions and more.

Learn More

Related Resources

Kollmorgen’s Direct Drive Technology Improves the Precision and Productivity of Lithium-Ion Battery Coaters >

Direct drive technology improves the manufacturing quality and productivity of lithium-ion batteries used in battery-electric vehicles and other products that are changing the world.
Kollmorgen Direct Drive Technology Enhances the Accuracy and Throughput of Electric Vehicle Battery Production

Kollmorgen Direct Drive Technology Enhances the Accuracy and Throughput of Electric Vehicle Battery Production >

As electric vehicles promise cleaner, more sustainable transportation, the need for reliable lithium-ion batteries is skyrocketing. Battery manufacturers are looking for innovative ways to maximize production quality and speed.
Cartridge DDR

Going Beyond Performance: Cost Savings with Direct-Drive Systems >

The performance benefits of direct-drive motors are well documented: industry-leading performance, improved accuracy, higher throughput, better reliability and quieter operations. This is because, unlike a conventional motion setup, a direct-drive…
Printing Machine

Direct Drive Motors Improve Flexographic Printing Performance >

Recent work done by Kollmorgen—a global leader in manufacturing motor and motion solutions—has shown that it is possible to synchronize components within the flexo printing process without mechanical transmission by using closed loop control…

Kollmorgen Is on the Perseverance Rover—And Extreme Environments Everywhere >

From the surface of Mars to the depths of the ocean, from the core of the earth to the core of the human body, Kollmorgen motion systems take on the most extreme environments.

How Does a Direct Drive Linear Servo Motor (Actuator) Work? >

A direct drive linear actuator, using a permanent magnet linear servo motor produces force and velocity based on the supplied current and voltage and provides a linear movement along the axis being driven. The linear servo motor works as part of a…
High Definition Cutting: The Kollmorgen Advantage

High Definition Cutting: The Kollmorgen Advantage >

Plasma, laser and waterjet cutting machines can have very different applications, but they all have one thing in common, they depend on precisely controlled motion. To achieve next-generation accuracy, efficiency and productivity, machine builders…
Material Forming Overview Brochure

Material Forming Overview Brochure >

Advanced material forming processes are defined by quality, repeatability and throughput. These requirements place unique demands on the performance of the motion systems that drive cutting, bending, braking and other material forming machines.
Automating Systems for Sheet Metal Forming, Kollmorgen

Automating Metal Forming Systems to Improve Productivity and Flexibility >

Learn how a major supplier of automated tube-cutting machines used direct-drive technology to transform metal-forming performance, precision and versatility. Get the details, and envision the possibilities for your own metal-cutting machine.