Kollmorgen Essentials adds a new eight-axis controller and high-voltage drive capability to right-size motion system builds for industrial applications.
Kollmorgen, a global leader in navigation and controls technology for automated guided vehicles (AGVs) and autonomous mobile robots (AMRs), announces the launch of NDC Layout Assistant ; a tool that provides fast, structured insight into layout…
Kollmorgen Corporation, a global leader in motion control and automation solutions, has expanded the application range of its Kollmorgen Essentials™ Servo Drive (KED) to include hygienic and washdown environments.
With ATEX and IECEx certifications, the new AKME Series brings Kollmorgen performance and versatility to hazardous locations including Zone 2 and 22 areas.
The latest SafeMotion Monitor™ firmware (SMM 3.0) expands functional safety for linear motors with EnDat 2.2 safe feedback support and SIL 3 compliance.
In many warehouses and production sites, the handover between manual labour and automated operations presents a daily challenge. Manually placed pallets are sometimes positioned off-coordinate, which creates problems for mobile robots that rely on…
Simplify motion engineering, speed up setup and minimize costs. Kollmorgen Essentials™ Motion Systems are optimized for precision servo performance and value.
Kollmorgen’s latest system release brings new capabilities to the NDC platform, making it easier to develop, deploy, and manage automated vehicles in a wide range of applications.
Kollmorgen, a global leader in navigation and controls technology for automated guided vehicles (AGVs) and autonomous mobile robots (AMRs), announces the launch of the AC7 and DC7 Motor Controllers, a powerful new generation of AC and DC motor…
Discover Kollmorgen’s new linear direct drive motor, engineered to move heavy loads with fast precision and to simplify machine design for the global marketplace.
Kollmorgen’s battery-free SFD-M encoder provides absolute 16-bit multi-turn positioning data at system power up with zero incremental cost. Eliminate homing sequences and maintain positioning accuracy through 65,536 complete motor revolutions for a…
The latest update to SafeMotion™ Monitor (SMM) firmware — SMM2.0 — enables use with a wider range of encoders for new high-performance applications.