Kollmorgen

Kollmorgen eNews

NORTH AMERICA | AUGUST 2011

  Kollmorgen on LinkedIn Kollmorgen on YouTube Kollmorgen on Facebook Kollmorgen on Twitter
     
space  

High-Performance in Small Package

Integrated motion and logic control

Today's machine builders are tasked with building more compact but increasingly productive and energy efficient machines. That combination demands more powerful and efficient motion control systems capable of delivering greater throughput and flexibility, with less downtime and within a smaller footprint. Kollmorgen can help.

AKM8

Kollmorgen's high-performance AKD™ servo drive and AKM™ servomotor combine to deliver maximum torque with minimal energy consumption, in a footprint that is up to 50 percent shorter than competitive servo solutions. And with the ability to provide inertia mismatches of greater than 500:1 from the base motor and drive system, Kollmorgen servo systems deliver extremely efficient and stable operation even in highly dynamic applications.

Learn More »

space
space  

High Throughput, Zero Maintenance Indexing Solutions

Performance advantage

Nowhere does motion matter more than in high-performance machines - and selecting the optimal solution for a given application requires far more than specifying individual high-performance components.

Kollmorgen recently worked with a packaging machine builder to solve a challenging form, fill and seal application that required rapid and highly reliable indexing. The implemented solution delivers move times of less than 100 ms with a corresponding 50 percent increase in throughput when compared with the previous motion system - all in a package that provides 10 year maintenance-free operation to maximize machine uptime and reduce total cost of ownership.

Learn more about this application - and Kollmorgen's holistic approach to motion system selection that combines co-engineering capabilities with a robust family of best-in-class components to solve even the most demanding application requirements - in our new video, Kollmorgen KBM™ Direct Drive Rotary Motor Indexing Application.

Watch Video »

space
space  

Learn How to Build a Better Converting and Packaging Machine at PACK EXPO

Model Based Design

Converting and package printing machine builders are tasked with building increasingly flexible and reliable machines that deliver ever-greater throughput. Success starts with selecting high-performance motion control solutions that drive measurable results.

Kollmorgen is exhibiting at the Converting & Package Printing Expo Pavilion co-located with PACK EXPO from September 26 - 28, 2011 at the Las Vegas Convention Center. We invite you to attend this powerful show and stop by to discuss your application needs, and to learn more about how we can work with you to co-engineer a superior performing machine.

Our blend of motion control expertise and products can help you achieve the tangible benefits that will give your converting or packaging machine a competitive advantage.

Find us in the South Building, Hall S2 at Booth 5970, or plan ahead by scheduling a meeting with one of our industry experts today.

space
 
 

In This Issue:

 
   
 

Upcoming Events:

 
 

Advanced Control Programming

 
 

September 20 – 24, 2011
Fond du Lac, WI

 
 

December 13 – 17, 2011
Fond du Lac, WI

 
 

Controls 101: ZMP SynqNet® Boot Camp

 
 

October 31 – November 4, 2011
Santa Barbara, CA

 
 

Controls 102: Troubleshooting Techniques for ZMP SynqNet® Motion Controllers

 
 

November 14, 2011
Santa Barbara, CA

 
 

Controls 201: MPI Programmer's Course

 
 

September 12 – 16, 2011
Santa Barbara, CA

 
 

December 5 – 9, 2011
Santa Barbara, CA

 
 

Controls 202: MPX Programmer's Course

 
 

October 3 – 4, 2011
Santa Barbara, CA

 
 

Controls 203: Advanced Servo Tuning and Motion System Analysis using Bode Tool

 
 

October 14, 2011
Santa Barbara, CA

 
 

Controls 301: Develop Advanced Control Algorithms with MechaWare™

 
 

October 17 – 21, 2011
Santa Barbara, CA

 
 

Motion Control Maintenance

 
 

November 3 – 5, 2011
Fond du Lac, WI

 
 

Motion Control Programming

 
 

September 13 – 17, 2011
Fond du Lac, WI

 
 

October 11 – 15, 2011
Fond du Lac, WI

 
 

November 8 – 12, 2011
Fond du Lac, WI

 
 

December 6 – 10, 2011
Fond du Lac, WI

 
 

Kollmorgen offers technical training courses throughout the year on a variety of subjects and product lines. Courses are designed and taught by key Kollmorgen personnel who are directly associated with the particular product or subject. These programs emphasize a practical, hands-on approach to learning. Customized, on-site technical training is also available. For more information, contact training@kollmorgen.com.


 

******

Subscribe to me on YouTube

Have you signed up at YouTube to get updates when new Kollmorgen videos are available?


It's fast and easy!


Subscribe today and get up-to-date access to our menu of videos that demonstrate real solutions that solve common engineering challenges and demanding applications requirements.

 
     
     

KOLLMORGEN     |     www.kollmorgen.com

©2011 Kollmorgen. All rights reserved.
This email was sent by: Kollmorgen
203A West Rock Road Radford, VA, 24141, USA

Update Profile and Subscription Preferences

Signup for the Kollmorgen eNewsletter