S-Curve Corner Transition – Design and CalculationsThe reason the S-Curve Corner Transition was designed was due to the existing Corner Distance Transition having a discontinuity in the acceleration vector when entering the circular arc of the transition. If the axes group is travelling in a line at constant speed, the acceleration vector is zero… | Jeanie |
İngilizce | |
CNC PPC - Registradores especiais do CNCLista de registradores especiais do CNC para acessar dados em tempo real, status do CNC e comandos. |
Will Gaffga |
Portuguese, Brazil | |
Retrofit KAS EtherCAT Backups with AKD2G FirmwareThe AKD2G drives with firmware versions 02-12-00-001 (and later) do not support downgrading the firmware to the versions 02-12-00-000 (or earlier). The KAS EtherCAT backups created using AKD2G firmware 02-12-00-000 (or earlier) are not capable of restoring the drive’s configuration once any AKD2G… | Jeanie |
İngilizce | |
AKD2G EtherCAT W7011 Warning and F7011 Fault Synchronization Error SupportThis article provides details related to cause and remedy of the W7011 warning and F7011 Fault in the AKD2G EtherCAT drive. |
toddevans01 |
İngilizce | |
Using Siemens PD_TEL9_DrivePos with Telegram 9 for Positioning with AKD2G Profinet RTThis document provides test results when using Siemens PD_TEL9_DrivePos function block with AKD2G Profinet Telegram 9 |
Will Gaffga |
İngilizce | |
KAS v4.01 Software is now available!! KAS v4.01 Software is now available!! |
dusty.schafer |
İngilizce | |
AKD and AKD2G Resolver Excitation Output Voltage Specification AKD and AKD2G Resolver Excitation Output Voltage Specification |
Will Gaffga |
İngilizce | |
AKD1G Reading Faults Over Ethernet IPDiscussion on methods for reading faults over Ethernet IP. |
toddevans01 |
İngilizce | |
AKD2G Controlled Stop and Holding Brake TimingThis is an explanation of the controlled stop and brake timing functionality in the AKD2G drive. |
Will Gaffga |
İngilizce |
Servo veya step motordan hangisine ihtiyacınız olduğunu bilmiyor musunuz?
İhtiyacınız olan desteği bulun
Kollmorgen Otomasyon Paketi Dinamik Hareket Kontrolüne Nasıl Yardımcı Olur?
Read MoreOlağanüstü mühendislik