Home tab
To access the KAS web server home page, enter the controller's IP address.
This page provides an overview of the device including:
- Manufacturer
- CPU Speed
- CPU Cores
- Model Number
- Serial Number
- Hardware Revision
- TCP/IP MAC Address: A unique value associated with the TCP/IP network adapter that uniquely identifies the adapter on a LAN.
- EtherCAT MAC Address: A unique value associated with the EtherCAT network adapter that uniquely identifies the adapter on an EtherCAT network.
-
-
Unless otherwise noted, any reference to AKD PDMM or PCMM refers to both the 800MHz and the single- and dual-core 1.2GHz variants.