Salta al contenuto principale

Kollmorgen Support Network

Benvenuto in Kollmorgen Support Network (precedentemente KDN). Trova i download, fai domande, unisciti alla community

 

 

Dati della community:
895
Contributi
Utenti registrati
1517
Articoli
2730
Download

Ultimi articoli

AKD2G System Configuration with Kollmorgen DDL Linear MotorsThis document shows the wiring requirements for connecting the DDL linear motors to the AKD servo drive. It also describes the setup procedure for configuring the AKD2G drive in the Workbench software.
toddevans01
AKD2G DS402 and Manufacturer Specific Torque and Current Setpoint and FeedbackFor AKD1G ECAT users the objects 2071h and 2077h do not exist. See the following app note for equivalents with the AKD2G ECAT drive.
toddevans01
S-Curve Corner Transition – Design and CalculationsThe reason the S-Curve Corner Transition was designed was due to the existing Corner Distance Transition having a discontinuity in the acceleration vector when entering the circular arc of the transition. If the axes group is travelling in a line at constant speed, the acceleration vector is zero…
Kollmorgen Support
CNC PPC - Registradores especiais do CNCLista de registradores especiais do CNC para acessar dados em tempo real, status do CNC e comandos.
Rodrigo Gallo Rodrigo Gallo
Retrofit KAS EtherCAT Backups with AKD2G FirmwareThe AKD2G drives with firmware versions 02-12-00-001 (and later) do not support downgrading the firmware to the versions 02-12-00-000 (or earlier). The KAS EtherCAT backups created using AKD2G firmware 02-12-00-000 (or earlier) are not capable of restoring the drive’s configuration once any AKD2G…
Kollmorgen Support

Discussioni recenti della community

Feature Request - KAS IDE
njandroep
profiles creation
jay thomas
Feature - Add a Description to Motion Tasks
njandroep
Homed reference point retained during power down?
njandroep
S400 Drive program COM1 fail
MolnaarBence

Risorse per il supporto online

Non trovi quello che ti serve? Di seguito sono disponibili ulteriori opzioni di assistenza, tra cui la documentazione completa per KAS e AKD, i link alla nostra area di formazione e i documenti per i fornitori.