Skip to main content

Monitoring and controlling brakes through on-drive functional safety technology

When one or more machine axes carries a vertical load, the safety of operators, products and the machine itself all depend on reliable braking. This is especially true when employees work in close proximity to highly automated equipment. Because gravity never compromises, you must never compromise. You need to provide a minimally disruptive way to monitor and test brake functionality on a regular basis.

However, safety standard ISO 13849-1 does not allow brake testing functions to be embedded into standard machine controls. So what are your options? How do you optimize the system to achieve the safety level you need? And how do you do it as simply and cost-effectively as possible. Read this white paper to understand the operation and advantages of on-drive safety functionality, such as offered by the AKD2G servo drive family.

 

Fill out this short form

to view this White Paper

-OR-

Login / Register

to gain access to Kollmorgen content

Privacy Statement - By sending us your contact details you agree that your personal data/user behavior can be electronically stored and processed. If you no longer wish to receive the enewsletter, you can unsubscribe at any time.

CAPTCHA

Five Motion Tips for Optimal High-Definition Metal Cutting Performance

Plasma, laser and waterjet cutting machines all have one thing in common: customers are looking for next-generation performance. When manufacturers purchase a new or upgraded machine, they’re focused on the capabilities that will allow faster, more reliable production of higher-quality products. That means your reputation and success as a machine builder depend on demonstrating the best performance, the best design and the best integration.

Learn More

2G Motion System: Best by Design

When you need optimal motion control, the intuitive solution is to choose best-inclass components, regardless of vendor mix. But as an engineer, you know that intuitive doesn’t always mean right.

Learn More

Engineer the Exceptional

Learn how to engineer exceptional machines, robots and vehicles with the highest-performing, most reliable motors, drives, automation solutions and more.

Learn More

Related Resources

Ground satellite 

AKD2G 24A Data Sheet >

Kollmorgen’s new AKD2G 24A servo drive delivers 3x the continuous current capacity and offers a rich feature set for simple integration in complex applications. 
Kollmorgen Express Delivery significantly shortens lead times for the company’s most popular motion products

Kollmorgen Express Delivery significantly shortens lead times for the company’s most popular motion products >

Motion leader Kollmorgen announces a new classification for select products that can be delivered within an accelerated timeframe.

5 Key Reasons to Consider an Upgrade to AKD2G Servo Drives >

Advances in processor technology for servo drives continue to expand the features and capabilities they offer. Choosing a new drive or control system over an existing system ultimately depends on the application requirements. The AKD2G servo drive…
AKD2G: Mentor Sessions

AKD2G Quick Setup with Safe Torque Off & Advanced Configuration with AKD2G Dual-Axis with Functional Safety >

The AKD2G drive is an easy to use, but comprehensive drive. The key to mastery is learning how to use the Workbench software.
AKD2G Setup: I/O, Motion Tasks, and the Scope Tool

AKD2G Setup: I/O, Motion Tasks, and the Scope Tool >

If you have some experience with the AKD or AKD2G, but want a little more in the form of a guided setup, then join us for this webinar. Learn best practices across all key steps of set-up, with the opportunity to ask your specific questions to our…

Implementing New AKD2G Drive Features  >

The Workbench software used to commission and optimize our new-generation AKD2G servo drives receives regular updates and new features. Curious about what’s new and how it might benefit your machine? Then this webinar is for you. Join us as Will…
10 SafeMotion™ Functions to Consider for Your Application

10 SafeMotion™ Functions to Consider for Your Application >

Famous last words: “Don’t stop the machine, I’ll just…” Manufacturers used to rely on physical barriers and total machine shutdown to protect workers. But with today’s high production quotas and thin margins, too many people are taking unnecessary…

How to Select a Servo Drive >

A servo drive should be selected based on the specific servo motor used in the application. Find out ho to select a servo drive for your application.

How Does a Servo Drive Work? >

A servo drive is an electronic device that is part of a closed loop system, producing current and voltage to rotate a servo motor. The closed loop system includes the servo drive, servo motor and feedback device, and is commanded from an analog or…