Passer au contenu principal

Réseau d'assistance Kollmorgen

Bienvenue sur le réseau d'assistance Kollmorgen (anciennement KDN). Recherchez des téléchargements, posez des questions et rejoignez la communauté

 

 

Statistiques du site :
872
Contributions
Utilisateurs enregistrés
1518
Articles
2743
Téléchargements

Derniers articles d'assistance

KAS v4.02 Software is now available!KAS v4.02 Software is now available!
Prashanth Morishetty
AKD2G System Configuration with Kollmorgen DDL Linear MotorsThis document shows the wiring requirements for connecting the DDL linear motors to the AKD servo drive. It also describes the setup procedure for configuring the AKD2G drive in the Workbench software.
toddevans01
AKD2G DS402 and Manufacturer Specific Torque and Current Setpoint and FeedbackFor AKD1G ECAT users the objects 2071h and 2077h do not exist. See the following app note for equivalents with the AKD2G ECAT drive.
toddevans01
S-Curve Corner Transition – Design and CalculationsThe reason the S-Curve Corner Transition was designed was due to the existing Corner Distance Transition having a discontinuity in the acceleration vector when entering the circular arc of the transition. If the axes group is travelling in a line at constant speed, the acceleration vector is zero…
Kollmorgen Support
CNC PPC - Registradores especiais do CNCLista de registradores especiais do CNC para acessar dados em tempo real, status do CNC e comandos.
Rodrigo Gallo Rodrigo Gallo

Derniers sujets de la communauté

profiles creation
jay thomas
Homed reference point retained during power down?
njandroep
S400 Drive program COM1 fail
MolnaarBence
Add new AKDn on existing AKDC
bcharpentier
Linear Motor Service mode
Tamim

Ressources d'assistance en ligne

Vous ne trouvez pas ce dont vous avez besoin ? Des options d’assistance supplémentaires, dont une documentation complète sur la KAS et l'AKD, un espace de formation et des documents fournisseurs, sont disponibles ci-dessous.