In this video in our ongoing "Two Minutes of Motion" series, Gordon covers connecting to the AKD2G Servo Drive with Workbench, I/O and motion task setup.
In this Two Minutes of Motion episode, Gordon elaborates on how the AKD Motion Task moves can be blended. Blending consecutive moves by matching velocity or acceleration allows the machine designer to optimize the motion profile to meet performance requirements.
Kollmorgen's AKD servo drive features a built-in Motion Task builder, allowing you to simplify even your toughest motion contol profiles with AKD Workbench. Watch how it works!
One of the new features in the latest release of AKD Workbench is how the interface works with multiple axes. Gordon provides a brief overview of these changes in this session of Two Minutes of Motion.
In the AKD Servo Drive, Workbench makes it easy to set the units to match your mechanism. In this Two Minutes of Motion segment, we show how to set up AKD units to match the motion of your screw mechanism
In this Two Minutes of Motion episode, Gordon provides an overview of how to set up Units for a Rack and Pinon Mechanism in the AKD servo drive using Workbench. Setting up units based on your mechanism helps speed up setup time and lets you work in units that make sense to your machine.
In the Two Minutes of Motion segment, we review how easy it is to configure units in the AKD Workbench environment, to make your application work go smoothly. You can even customize units so as you set your Motion Task, you work in the units of you actual mechanics.
Customize your units with Kollmorgen's AKD servo drive. Check out this Two Minutes of Motion segment on how to set up a belted or geared belt conveyor in units that work for your motion control application.