Check out this Why Motion Matters segment on how Kollmorgen helped Packaging Progressions Inc. improve machine performance by reducing machine cleaning time, improving machine reliability, and helping reduce the potential risk for food recall - all with the AKMH hygienic servo motor.
Application that minimizes operational costs in a highly automated warehouse. In the very narrow aisle racking area, automated warehouse trucks handle the pallets. The warehouse trucks were automated with technology from Kollmorgen.
Application that automated the transportation of dairy goods from the prodution area to chilled storage. The forklifts were automated with technology from Kollmorgen.
Borealis in Stenungsund, a provider of polyolefin compounds, uses AGVs to minimize operational cost and damage to goods in their production plant. Rocla has delivered the system which is based on Kollmorgen’s AGV controls technology.
The AGV system at the hospital in Brive-la-Gaillarde has expanded into a new building. The system controls vehicles in the old building using inductive wire navigation and vehicles in the new building using natural navigation. The new navigation technology simplifies the expansion of systems since no changes are needed in the infrastructure.