Skip to main content

* All webinars are presented in English, unless otherwise noted.

*Classroom courses are taught in English and in-person at our office in Radford, Virginia, USA, unless otherwise noted.

Painless Frameless: Implementing and Installing Frameless Motors >

Webinar

Are traditional motors constraining your machine design? Motors don’t have to be bulky to create dynamic motion. Frameless motors allow you to keep your sleek machine design, and they are easy to implement. Join us for this highly popular event—now…

Painless Frameless: Implementing and Installing Frameless Motors - India >

Webinar

Are traditional motors constraining your machine design? Motors don’t have to be bulky to create dynamic motion. Frameless motors allow you to keep your sleek machine design, and they are easy to implement. Join us for this highly popular event—now…
English, IN

Preventing Electromagnetic Interference in Servo Cables >

Webinar

In servo systems, power cables that transmit electrical current to the motor run in close proximity to the feedback cables responsible for transmitting position and velocity data. Even with cables encased in protective jackets, magnetic fields…

Resolving Servo Feedback Choices >

Webinar

Is servo feedback the key to system performance? The role of feedback is to constantly send motor performance data to the drive, which uses this information to continually adjust servo commands. Selecting the wrong feedback device can have…

Scegliere in modo semplice il motore ideale per applicazioni in ambienti a rischio: Zona 2 e Zona 22  >

Webinar

Progettare soluzioni di motion per ambienti a rischio di esplosione non deve essere né complesso né costoso. In questo webinar tecnico scoprirai come i nuovi servomotori, azionamenti e cavi AKME di Kollmorgen, basati sulle prestazioni collaudate…
Italian

Signs You Should Consider a Frameless Motor in Your Machine >

Webinar

Big machines require big solutions. Right? But what if higher-performance machines could benefit from compact, space-saving, lightweight, more efficient embedded solutions? Did you know that high-performance applications for harsh environments like…
English, IN

Signs You Should Consider a Frameless Motor in Your Machine >

Webinar

Big machines require big solutions. Right? But what if higher-performance machines could benefit from compact, space-saving, lightweight, more efficient embedded solutions? Did you know that high-performance applications for harsh environments like…

Simplify Regen Resistor Selection for Motion Systems  >

Webinar

The power generated by a motor during deceleration can be detrimental to your motion system. To intercept this electrical power and prevent system harm, the use of a regeneration resistor is often required. Sizing and selecting the correct regen…

Step by Step Programming for AKD BASIC >

Webinar

Are you looking to get the most out of your AKD BASIC drive? The AKD BASIC drive combines the performance features of our leading AKD series along with built-in machine and motion control to deliver exactly what you're looking for. Using the…

Step by Step Programming for AKD BASIC >

Classroom Training

Hands-on programming for real world applications. This on-line course covers the building blocks required to develop programs for AKD BASIC. This course requires a demo drive (rent or purchase) and access to the internet. $300/Student

Step Into Motion: Best Applications for Stepper Technology >

Webinar

Each axis of motion has different requirements and while some need full servo control, many can be economically solved with stepper motors. Wondering when to use one vs. the other? Wondering which stepper is your best option? Kollmorgen motion…

Step Into Motion: The 411 on Stepper Technology >

Webinar

No need to call information to learn about step motion. Each axis of motion has different requirements, and while some need full servo control, many can be economically solved with stepper motors. Wondering when to use one technology versus the…