Skip to main content

* All webinars are presented in English, unless otherwise noted.

*Classroom courses are taught in English and in-person at our office in Radford, Virginia, USA, unless otherwise noted.

Motioneering: Creating Advanced Motion Profiles >

Webinar

In “Creating Advanced Motioneering Profiles” you build from the previous module and will expand into sizing more mechanism types: conveyor system and electric cylinder, to illustrate how to build complex motion profiles.In this session you'll learn…

Motor Topology options for EO/IR Applications >

Webinar

Go big or go long? Motor choice is about balancing the need for torque, form factor, and performance. Beyond length and diameter, learn how other motor topologies optimize your EO/IR platform.Key talking points:Reasons to adjust OD to through bore…

Motor Windings: Understanding ​How They Work and Affect Performance​​​  >

Webinar

Electric motors serve as the powerhouse ​driving industrial machinery, advanced robots, medical imaging systems and countless​ ​other ​applications​.​ ​I​ntricate ​copper ​windings play a ​fundamental​ role in ​motor​ operation​, with specific…

Motori frameless: less is more. Scopri come aumentare le prestazioni, semplificando la progettazione (session 1) >

Webinar

Questo webinar in due sessioni, rivolto a ingegneri, progettisti e tecnici, approfondirà le dinamiche che influenzano le prestazioni dei sistemi di trasmissione Motion e le tecniche di ottimizzazione.Esploreremo le tecnologie di feedback disponibili…
Italiano

Motori frameless: less is more. Scopri come aumentare le prestazioni, semplificando la progettazione (session 2) >

Webinar

Questo webinar in due sessioni, rivolto a ingegneri, progettisti e tecnici, approfondirà le dinamiche che influenzano le prestazioni dei sistemi di trasmissione Motion e le tecniche di ottimizzazione.Esploreremo le tecnologie di feedback disponibili…
Italiano

Neue Designmöglichkeiten mit gehäuselosen Motoren erschließen >

Webinar

Gehäuselose Motoren definieren neu, was im modernen Maschinenbau möglich ist. Durch die Kombination verschiedener rahmenloser Komponenten in einem einzigen Gehäuse erhalten diese Aktuatoren erhebliche Vorteile wie reduzierte Abmessungen, geringeres…
Deutsch

Next-Generation Motor Design for Missiles >

Webinar

Next-generation defense systems require next-generation motion capabilities. Commercial off-the-shelf motors seldom meet the design requirements of guided munitions and hypersonic missiles that must reach the target with precision despite extremes of…

On the Move with Low-Voltage Motors  >

Webinar

Technology is on the move. Battery-operated motors enable engineers to incorporate industrial automation processes on mobile platforms. Market trends are constantly advancing the need for sophisticated mobile robots, portable medical equipment and…

Optimizing Industrial Communication Using Fieldbus Technology and Kollmorgen Solutions  >

Webinar

As technology advances, there is an increasing need for efficient communication, centralized control, and real-time data exchange in industrial operations. Fieldbus systems enable various devices such as sensors, actuators and controllers to…

Ottimizza gli spazi e la modularità con la soluzione di azionamenti nearby di Kollmorgen >

Webinar

I quadri elettrici occupano spazio prezioso, che può essere utilizzato diversamente. Con la soluzione di azionamenti decentralizzati AKD-N di Kollmorgen, puoi superare le limitazioni dei motori con azionamento integrato e godere di prestazioni…
Italiano

Ottimizza la gestione dell’energia rigenerata dalla tua applicazione  >

Webinar

La potenza rigenerata da un motore durante la fase di decelerazione può essere dannosa per il sistema motion. La gestione di questa energia, al fine di prevenire danni al sistema, può essere affrontata con vari approcci, tra cui l’utilizzo di una…
Italiano

P8000 Stepper Drive Setup >

Classroom Training

This class provides an overview of the KAS and PCMM controller products with hands-on application of the Integrated Development Environment (IDE), Runtime, and adaption to AKD drives. Also included is the introduction to the IEC61131 programming…