Skip to main content

* All webinars are presented in English, unless otherwise noted.

*Classroom courses are taught in English and in-person at our office in Radford, Virginia, USA, unless otherwise noted.

Next-Generation Motor Design for Missiles >

Webinar

Next-generation defense systems require next-generation motion capabilities. Commercial off-the-shelf motors seldom meet the design requirements of guided munitions and hypersonic missiles that must reach the target with precision despite extremes of…

On the Move with Low-Voltage Motors  >

Webinar

Technology is on the move. Battery-operated motors enable engineers to incorporate industrial automation processes on mobile platforms. Market trends are constantly advancing the need for sophisticated mobile robots, portable medical equipment and…

Optimizing Industrial Communication Using Fieldbus Technology and Kollmorgen Solutions  >

Webinar

As technology advances, there is an increasing need for efficient communication, centralized control, and real-time data exchange in industrial operations. Fieldbus systems enable various devices such as sensors, actuators and controllers to…

Optimizing Motion Profiles for Minimum Torque Requirements and Cycle Times >

Webinar

The motion profiles triangular and 1/3 trapezoid are ​commonly ​used for their simplicity of design. ​However, using​ a triangular profile can be too aggressive in many systems, and a 1/3 1/3 trap doesn’t always provide the traverse time needed to…

Ottimizza gli spazi e la modularità con la soluzione di azionamenti nearby di Kollmorgen >

Webinar

I quadri elettrici occupano spazio prezioso, che può essere utilizzato diversamente. Con la soluzione di azionamenti decentralizzati AKD-N di Kollmorgen, puoi superare le limitazioni dei motori con azionamento integrato e godere di prestazioni…
Italiano

Ottimizza la gestione dell’energia rigenerata dalla tua applicazione  >

Webinar

La potenza rigenerata da un motore durante la fase di decelerazione può essere dannosa per il sistema motion. La gestione di questa energia, al fine di prevenire danni al sistema, può essere affrontata con vari approcci, tra cui l’utilizzo di una…
Italiano

P8000 Stepper Drive Setup >

Classroom Training

This class provides an overview of the KAS and PCMM controller products with hands-on application of the Integrated Development Environment (IDE), Runtime, and adaption to AKD drives. Also included is the introduction to the IEC61131 programming…

Painless Frameless: Implementing and Installing Frameless Motors >

Webinar

Are traditional motors constraining your machine design? Motors don’t have to be bulky to create dynamic motion. Frameless motors allow you to keep your sleek machine design, and they are easy to implement. Join us for this highly popular event—now…

Painless Frameless: Implementing and Installing Frameless Motors - India >

Webinar

Are traditional motors constraining your machine design? Motors don’t have to be bulky to create dynamic motion. Frameless motors allow you to keep your sleek machine design, and they are easy to implement. Join us for this highly popular event—now…
English, IN

Preventing Electromagnetic Interference in Servo Cables >

Webinar

In servo systems, power cables that transmit electrical current to the motor run in close proximity to the feedback cables responsible for transmitting position and velocity data. Even with cables encased in protective jackets, magnetic fields…

Resolving Servo Feedback Choices >

Webinar

Is servo feedback the key to system performance? The role of feedback is to constantly send motor performance data to the drive, which uses this information to continually adjust servo commands. Selecting the wrong feedback device can have…

Scegliere in modo semplice il motore ideale per applicazioni in ambienti a rischio: Zona 2 e Zona 22  >

Webinar

Progettare soluzioni di motion per ambienti a rischio di esplosione non deve essere né complesso né costoso. In questo webinar tecnico scoprirai come i nuovi servomotori, azionamenti e cavi AKME di Kollmorgen, basati sulle prestazioni collaudate…
Italian