Back to top

Success Stories

Better Cut Quality Through Improved Connectivity, Kollmorgen
29 Jun 2020

A Turkish-based company was looking to improve the cost, cut quality and machine serviceability of their flagship plasma cutting machine. Kollmorgen engineers implemented an AKM/AKD system solution to provide faster indexing and settle times. By implementing advanced tuning, the machine dramatically improved cut quality.

Simplified Controller Integration Speeds Time-to-Market, Kollmorgen
29 Jun 2020

The market for plasma cutting machines in North America is highly competitive, with customers looking for a variety of solutions—from big machines with high capacity and throughput to smaller machines for fabrication shops with more limited resources. A machine builder in Mexico looked for new ideas to successfully grow in this challenging environment. Success with the small, large, upgraded and custom machines all depended on precise motion, achieved quickly, affordably and reliably. That’s where Kollmorgen came in.

Kollmorgen Enhancing Precision While Reducing Size, Weight and Cost
29 Jun 2020

A major manufacturer of advanced laser-cutting machines engaged Kollmorgen in the early 1980s, recognizing the importance of precision motion to meet the unique and varied requirements of the machine builder's customer base. Kollmorgen designed a customized winding that worked with a specialized, high-density magnet material to deliver the needed power with no need to change the installation footprint.

Peening extends life
22 Apr 2019

Freymatic is building shot peening plants for the construction of aircraft engines – and, to do this, it's opting for Motion Control by KOLLMORGEN to achieve high quality requirements

B8 Model MELD Machine
01 Feb 2019
MELD Manufacturing achieved major breakthroughs in materials additive manufacturing with MELD technology – a solid-state process that requires no melting used to manufacture and repair parts. Throughout the development process, Kollmorgen engineers and MELD Manufacturing worked together to achieve optimum precision and power.
30 Jan 2019
Keiding, Inc., leverages AKD® servo drives and AKM64L servo motors on a new molding machine to fuel state-of-the-art molded fiber packaging.
Virtual reality and servo motors: a dynamic partnership
20 Jun 2018

With efficient torque density, the 3 DOF platforms powered by KOLLMORGEN Servo for a VR roller coaster become reality.

Alesa - Grinding Machine - Cutting edge: The shark’s teeth
02 Oct 2017
Saw blade manufacturer Alesa develops its own grinding machine with Washdown servo motors from KOLLMORGEN with single-cable connection technology.
18 Sep 2017
Direct drives with braking modules from KOLLMORGEN provide noticeable energy savings in coil handling.
23 Jun 2017

For the pre-ferment, Bühler has developed a solution - JetMix - Better hygiene thanks to KOLLMORGEN’s stainless steel servo motor