Back to top

Success Stories

KOLLMORGEN FREYMATIC LeanCut Machine Brick Industry
15 Apr 2019

Motion Control by KOLLMORGEN makes fast and precise cuts from the column of clay

Kollmorgen success story: The precise geometry of 3D cutting
15 Mar 2019

KBM motors as a byword for accuracy in laser cutting

Kollmorgen - 3D Cutting for large formats
22 Feb 2019

Success Stories: Kollmorgen frameless direct drive linear motors for metal cutting

B8 Model MELD Machine
01 Feb 2019
MELD Manufacturing achieved major breakthroughs in materials additive manufacturing with MELD technology – a solid-state process that requires no melting used to manufacture and repair parts. Throughout the development process, Kollmorgen engineers and MELD Manufacturing worked together to achieve optimum precision and power.
30 Jan 2019
Keiding, Inc., leverages AKD® servo drives and AKM64L servo motors on a new molding machine to fuel state-of-the-art molded fiber packaging.
Safe Torque Off (STO) in practice: a Swiss manufacturer of test equipment is already using the TÜV-certified safety technology based on a slip ring and AKD-N servo drives from KOLLMORGEN arranged in a distributed setup.
02 Jan 2019

Safe Torque Off: Kollmorgen and Stemmann-Technik are developing a TÜV-certified solution

Servo drives simulate road behavior
26 Nov 2018

IMS Gear relies on KOLLMORGEN’s Motion Control solution for its test bench technology.

NDC Solutions, Kollmorgen, Yeefung
05 Sep 2018

Yeefung, an AGV partner to Kollmorgen, has developed a new generation of their car parking robot.

Kollmorgen NDCSolutions, High Reach AGV in Solar Panel Manufacturing
02 Jul 2018
Seraphim Solar System have improved accuracy and efficiency in their warehouse by introducing AGVs.
Virtual reality and servo motors: a dynamic partnership
20 Jun 2018

With efficient torque density, the 3 DOF platforms powered by KOLLMORGEN Servo for a VR roller coaster become reality.