Back to top

PLC Programming for Kollmorgen Automation Suite™

A complete graphical toolkit for PLC programming is included with Kollmorgen Automation Suite™, with support for all IEC 61131-3 programming languages. It’s fully integrated with motion programming, hardware setup and configuration, testing and debugging, HMI development, network setup and other development tools, so there’s only one software package to learn and use, and only one programming and configuration file to maintain.

Global
Product available worldwide
Kollmorgen Programmazione PLC IEC 61131-3 KAS_l.png
Industry 4.0 Ready

Features

  • Open architecture provides consistent support for both IEC 61131-3 and user-defined programming constructs in a single environment
  • Graphical, drag-and-drop programming environment ensures consistency and convenience
  • Programmed modules can easily be modified and reused, increasing development speed
  • Auto-recognize feature automatically brings Kollmorgen controllers, I/O devices, drives, motors and other hardware components into the development environment
  • Programming language interchangeability allows seamless integration of different languages for different programming tasks, and even translates one IEC 61131-3 language to another

Software-KAS-Diagram1

  • Offline development and simulation capabilities allow you to create and test solutions without deploying the target hardware or putting physical components at risk

Software-KAS-Diagram2

  • Graphical cam editor makes it easy to import, create, modify and reuse complex cam profiles

Software-KAS-Diagram3

  • Multi-variable software oscilloscope and standard debugging features simplify troubleshooting and fine-tuning

Software-KAS-Diagram4

Benefits

  • Quickly create, optimize and validate motion components and templates
  • Reuse and customize function blocks to suit many different applications
  • Customize the development environment to suit your working style
  • Simplify programming of complex automation systems that incorporate multiple types of components and configurations
  • Integrate PLC programming within the same environment you use to define system topology, auto-discover and auto-configure components, create cam profiles, test and debug motion programs, and more

Get Started

Count on Kollmorgen support to help you design and build a successful machine and keep it reliably productive, anywhere in the world. Our co-engineering experts will work with you to tailor a perfect-fit solution for your motion requirements.

Talk to a motion expert
Article
PLCopen Camming with KAS IDE software videos Series of three videos showing how to add camming to a PLCopen project in the KAS IDE with a PDMM or PCMM controller. The first video shows how to use the cam creation tool in the KAS IDE to create a...
Firmware Installation for AKI-CDB Panels Firmware on an AKI-CDB Panel can be loaded either by Ethernet or by USB. Setup if Loading via Ethernet  If loading via Ethernet, make sure that the computer IP address is in the same range...
Links to KAS Videos, Application Notes, and Sample Projects There are a number of KDN articles that contain videos, application notes, and demo programs to teach new users or refresh experienced users how certain features work. Below are links to these...
Getting Started with a KAS IDE Project Template The following video details how to get started with the KAS IDE (Integrated Development Environment) that is used to create PxMM controller application software. It includes: Open and...
Windows 10 - Win10 Screen Resolution Partial Descriptions Shown Below is a sample of a new project that has been opened in KAS/Win10. Some descriptions are cut off. One solution: “Pin” the Kollmorgen IDE to the start menu Used a right mouse click...

Pages