Skip to main content

Kollmorgen Support Network

Welcome to the Kollmorgen Support Network (formerly KDN). Find downloads, ask questions, join the community of your peers

Site Statistics:
112
Contributions
Registered Users
1524
Articles
2775
Downloads

Latest Support Articles

Processo de Tuning do Drive ABD em Eixos Horizontais e VerticaisOs servo-motores são controlados por drives que utilizam um método chamado de malha de controle.  A malha executa um cálculo com a realimentação da posição do motor e o valor de comando, visando reduzir ao máximo o erro através do ajuste dos ganhos. Ao final do ajuste tem-se como resultado a…
Christian Andrade
KAS v4.03 Software is now available!KAS v4.03 Software is now available!
Prashanth Morishetty
PCMM2G and PCMM Error and Alarm MessagesPCMM2G and PCMM Error and Alarm Messages
Jeanie
AKD2G EtherNet/IP Cyclic IO Assemblies and Explicit MessagingThe following demonstrates the different command types supported by the AKD EtherNet/IP drive for the Standard Assemblies and Connection. Many customers using a non-AB PLC or other EtherNet/IP device have found the following application note useful.
toddevans01
AKD1G EtherCAT Touchprobe ExamplesThis application notes shows the PDO mapping of and usage of AKD1G EtherCAT Touchprobes for position capture and demonstrates by example different trigger methods.
toddevans01

Latest Community Topics

Online Support Resources

Not finding what you need? Additional support options including thorough documentation for KAS and AKD, links to our training area, and supplier documents are available below.