Site Statistics:
872
Contributions Registered Users
1521
Articles2752
DownloadsLatest Support Articles
AKD2G EtherNet/IP Cyclic IO Assemblies and Explicit MessagingThe following demonstrates the different command types supported by the AKD EtherNet/IP drive for the Standard Assemblies and Connection. Many customers using a non-AB PLC or other EtherNet/IP device have found the following application note useful. |
toddevans01 |
|
AKD1G EtherCAT Touchprobe ExamplesThis application notes shows the PDO mapping of and usage of AKD1G EtherCAT Touchprobes for position capture and demonstrates by example different trigger methods. |
toddevans01 |
|
AKD1G EtherCAT Default Interpolated Position Mode and CSP Presentation and VideosThe PowerPoint presentations may be used in tandem with its respective video which cover using TwinCAT3 and the defaults from the ESI file (Interpolated Position mode) and additionally changing the default setup for Cyclic Synchronous Position mode. |
toddevans01 |
|
KAS v4.02 Software is now available!KAS v4.02 Software is now available! |
Prashanth Morishetty |
|
AKD2G System Configuration with Kollmorgen DDL Linear MotorsThis document shows the wiring requirements for connecting the DDL linear motors to the AKD servo drive. It also describes the setup procedure for configuring the AKD2G drive in the Workbench software. |
toddevans01 |
Latest Community Topics
profiles creation | jay thomas |
|
Homed reference point retained during power down? | njandroep |
|
S400 Drive program COM1 fail | MolnaarBence |
|
Add new AKDn on existing AKDC | bcharpentier |
|
Linear Motor Service mode | Tamim |
Latest Webinars & e-Learning
Online Support Resources
Not finding what you need? Additional support options including thorough documentation for KAS and AKD, links to our training area, and supplier documents are available below.