Skip to main content

Kollmorgen Support Network

Welcome to the Kollmorgen Support Network (formerly KDN). Find downloads, ask questions, join the community of your peers

 

 

Site Statistics:
113
Contributions
Registered Users
1523
Articles
2761
Downloads

Latest Support Articles

KAS v4.03 Software is now available!KAS v4.03 Software is now available!
Prashanth Morishetty
PCMM2G and PCMM Error and Alarm MessagesPCMM2G and PCMM Error and Alarm Messages
Jeanie
AKD2G EtherNet/IP Cyclic IO Assemblies and Explicit MessagingThe following demonstrates the different command types supported by the AKD EtherNet/IP drive for the Standard Assemblies and Connection. Many customers using a non-AB PLC or other EtherNet/IP device have found the following application note useful.
toddevans01
AKD1G EtherCAT Touchprobe ExamplesThis application notes shows the PDO mapping of and usage of AKD1G EtherCAT Touchprobes for position capture and demonstrates by example different trigger methods.
toddevans01
AKD1G EtherCAT Default Interpolated Position Mode and CSP Presentation and VideosThe PowerPoint presentations may be used in tandem with its respective video which cover using TwinCAT3 and the defaults from the ESI file (Interpolated Position mode) and additionally changing the default setup for Cyclic Synchronous Position mode.
toddevans01

Latest Community Topics

Online Support Resources

Not finding what you need? Additional support options including thorough documentation for KAS and AKD, links to our training area, and supplier documents are available below.