Back to top

workbench parameters different in simulated vs online mode

0 votes
+ vote
Vote up!

I appear to be getting a difference in the motor parameters depending on the online status.  I have a wbp file saved from the drive that displays a different set of axis motor property parameter values when in simulate mode compared to an online screenshot several days old.  I’m trying to determine if the parameters have actually changed since the screenshot was taken or if I’m not familiar with how Workbench operates.  I don't currently have access to the machine to verify online status.

 

Other details: using Workbench version 2.7, the motor autoset value is “1-On”, Device Model AKD-P00307-NBAN-0000, actual motor (not specified in simulate mode) AKM2G-21D-ANDNCA00

0 Comments

1 Answer

0 votes
+ vote
Vote up!

Chris:

We just talked on the phone? I did think of one thing. If your looking at the motor setup page in workbench, unless you had disabled the motor autoset and manually selected the motor, you could be looking at the default parameter settings?

Dan Wolke

0 Comments
ANSWER THIS QUESTION
You may login with either your assigned username or your e-mail address.
The password field is case sensitive.

If you do not have an account, click here to register.