Back to top

Workbench GUI doesn't display correctly.

0 votes
+ vote
Vote up!

I can't see some information on Workbench since I changed laptop. OS is Windows10 (Japanese) .  What is the root cause? Please see following screenshots.

image

image

image

Comments

See answer

didier.kuttel - Sun, 10/14/2018 - 07:09
Log in or register to post comments

1 Answer

0 votes
+ vote
Vote up!

Some views in WorkBench are still using WinForms. This technology does not support well the DPI scaling, we are migrating the application towards WPF a more recent technology handling much better the different DPI scaling.
To get rid of these problems, you can set back the scaling of your display to 100% - by default Win 10 is adapting the scaling based on the density of your screen.

To adjust the scaling at 100%, you can do this by right clicking on the Desktop and selecting Display Settings. From that dialog you can adjust the scaling with the “Change the size of text, apps, and other items” slider. You may need to log out and log back in to your account to see the effect.

More details here (option 1):
https://www.tenforums.com/tutorials/5990-change-dpi-scaling-level-displays-windows-10-a.html
 

0 Comments
ANSWER THIS QUESTION
You may login with either your assigned username or your e-mail address.
The password field is case sensitive.

If you do not have an account, click here to register.