What is Available AC Input Range for AKD Drive?
According to the homepage of Kollmorgen, there is a voltage rage(187 ~ 528V) as the below picture..
Could you please let me know what mean this range? Can I use ac line voltage from 187 to 528 Vac?
http://www.kollmorgen.com/en-us/products/drives/servo/akd/
Comments & Answers
Joerg Muslewski said ...
Please refer to AKD Installation Manual, chapter 7.6 "Electrical Data AKD-xzzz07".
There you will find the information about the rated supply voltage values.
The voltage range on our homepage presents absolute minimum and maximum values.