Back to top

Getting Started

New to KDN? Here are a few tips to help you get answers quickly.

Check the Knowledge Base or Search. Your question may already be answered.

Can't find the answer to your question? Ask! Post a question to get answers from the community

Include details. What hardware, firmware, operating system, and software version are you using? Include a screenshot of the problem, when possible.

Latest Posts

Joe Parks's picture
Joe Parks
5 days 6 hours ago

AKD2G Dual Axis drives have the ability to use the new Gantry Command Source. When the Command Source is changed to 4 - Gantry, Axis2 will follow all commands sent to Axis1 (enable/disable and motion commands). This is meant to be used when there are gantry mechanics and both Axis1 and Axis2 are physically connected and sharing a load. By giving them the same motion commands at the same time ensures that they will not fight each other while connected and prevent binding of the mechanics.

Leonardo Souza's picture
Leonardo Souza
1 month 4 days ago

As séries ABD® (Altra Brasil Drive) e ABM® (Altra Brasil Motor) são a linha completa de servo-acionamentos com base em EtherCAT, desenvolvida exclusivamente para o mercado brasileiro. Essa linha de produtos possui grande competitividade e ótima relação custo-benefício, garantidas através da integração com os controladores Kollmorgen (KAS & PPC).

image

Ann Pater's picture
Ann Pater
2 months 1 week ago

This article discusses common questions about the differences between AKD and AKD2G drives. A PDF version of these questions is attached below. More information can be found in the online help under the topic AKD2G vs. AKD.

Ariesta Wibisono's picture
Ariesta Wibisono
2 months 2 weeks ago

The S200 updated boards use a larger FPGA with multiple feedback and filter options. Two new parameters have been introduced to select/set these options. These parameters allow the updated boards to use a single FPGA control logic release (LogicVer = 4/VerLW = 4.xx) to replace multiple control logic versions used in original S200 units with old FPGA (LogicVer = 3/VerLW = 3.xx) up to 2021.