Skip to main content

Kollmorgen Support Network

To better serve our Kollmorgen users with questions too complex to be addressed in this space, we made the painful decision to close this Community forum.

Please submit your question using the contact us form to reach our application engineering team.

For the immediate future, you can still access and read past posts.

Thank you for understanding and for participating in the community over the years.

Using the ICH Performance Curves | 29 Mar 2017 | |

Using the ICH Performance Curves

How do I unlock the ICH motor performance curves so that I can develop the curves?  It seems password protected even though it's posted on KDN and seems to be something we could allow someone to edit.

 

What I want is a PC based on AKD6A HV, with a ICH33-050-A1 & ICH22-075-A1

Comments & Answers

jcoleman02 said ...

jcoleman02 | Thu, 03/30/2017 - 14:42

I just downloaded the "ICH motors performance curves 2016-10-11.zip" file from KDN.  I copy/pasted the excel file to a folder, opened it, selected the ICH22-075-A1 and selected 640 for the bus voltage.  There is no password required.  See the attached screenshot.

sitz_KDN | Wed, 03/29/2017 - 19:25

I meant to add 480VAC.

About this Question

sitz_KDN
Taxonomy: