Skip to main content

Kollmorgen Support Network

Back EMF >

Back Electro-motive Force is the voltage generated during the operation of a rotating machine (a generator or a motor). When voltage (an electro-motive force) is applied to a motor's armature, it begins to rotate, and an amount of electrical…

VSTART Parameter (S300-S700) >

ASCII - Command VSTART     Syntax Transmit VSTART [Data]     Syntax Receive

MUR Parameter (S300-S700) >

ASCII - Command MUR     Syntax Transmit MUR [Data]     Syntax Receive MUR <Data>  

Motor Inductance >

Valid for S300, S400, S600, S700

AKD Power Connector >

Used with AKD, voltage type 06, current types 3A and 6A Used with AKD, voltage type 06, current types 12A and 24A, and with AKD voltage types 07, current types 3A to 24A

Forming >

Valid for AKD, S300, S400, S600, S700 Capacitors integrated in servo amplifiers may be uncharged to absolute zero level, if servo amplifiers are stored for longer than a year without being connected to mains voltage. If rated voltage is…

Residual Current Protective Device >

Table of Contents General Function Use with servo amplifiers Fault Current Leakage current

Voltage Rating >

Voltage rating for cables varies between standards. Typical voltage ratings for cables are 300V and 600V. CE requires the equipment or other installations to have insulation rating equal to the maximum circuit voltage applied to any conductor within…
Subscribe to Voltage