The attached video covers important topics such as ESI (XML) file acquisition and importation into TwinCAT 3. Basic setup and motion from the TwinCAT 3 console are also demonstrated. Finally how to recognize and resolve a mismatch…
The touch probe feature of EtherCAT is simply a position capture. In fact, it uses the position capture feature in the AKD. When touch probe is set up and enabled, it automatically configures and arms the AKD’s position capture. …
Valid for S300, S700
Introduction
Since version 2.3.1 of the DriveGUI it's possible to communicate via the TwinCAT PLC. It's possible to communicate with both TwinCAT versions: 2.x or 3.x. Due to the efficient implementation of ADS-messaging…