Skip to main content

Kollmorgen Support Network

Boot Time of AKD / AKD2G >

The boot time was measured from the point of applying 24V control power to the drives.  The time was measured to specific indicators and functions of the drives. Note that AC power was already turned on prior to running these tests, so that the…

MC_TouchProbe and Time-Based Capture >

When using time-based capture with MC_TouchProbe, one may find that the accuracy of the captured position depends on the travel velocity of the captured axis.

MTIME Parameter (S300-S700) >

ASCII - Command MTIME     Syntax Transmit MTIME [Data]     Syntax Receive MTIME <Data>  
Subscribe to Time