Back to top

What is the update rate in the AKD of reading the motor temp sensor through the SFD feedback?

The standard operating temperature of an AKM is based upon the most temperature sensitive device.  This is typically the bearings .  The standard bearings that are used on the AKM put the operating temperature at -20 to +120 deg.

ASCII - Command TEMPMFILT