Skip to main content

Kollmorgen Support Network

TCP/IP Send and Receive in KAS Project >

Starting with the 3.04 release of KAS there are PLC function blocks to send or receive data with TCP/IP communication. The below video goes through the two attached sample programs. One is a program with TCP/IP receive function blocks that in the…

Communicating with the AKD over Telnet using HyperTerminal and PuTTY >

Normally, the Workbench software is used to connect to and configure the AKD drives.  However, there may be some instances where Workbench can't be used or where another communication method is preferred for troubleshooting purposes, etc. …

ProfiNet >

General PROFINET ( Pro cess Fi eld Net work) is the Profibus & Profinet International (PI) open industrial Ethernet standard for automation. There are two types Profinet types, Profinet CBA and Profinet IO:
Subscribe to TCP/IP