This sample configuration illustrates setting up a dual-axis AKD2G with dual-axis KSM 12-2 Safety PLC.
Safety Engineering is not so simple that one design will meet SIL2 for all applications. The intent of this document is to give a…
Implementation of STO Inputs
There are two types of STO input in common use today:
DC-DC Type: isolated STO input based on using a DC-DC converter to power the date driver circuitry.
O-C Type: opto-isolated input of a drive that acts upon…
This article will help you understand the differences between older S700 (S701-724) drives with single-channel STO and newer dual-channel STO S700 drives.