Skip to main content

Kollmorgen Support Network

S300, S700 ROFFSABS, Absolute Encoder Single Turn >

When configuring the S700 or S300, homing with an absolute encoder you will need to use ROFFSABS. ROFFSABS provides the necessary offset when physically homing. Single Turn Absolute is absolute to 1 rotation of the motor. To home the drive with an…

Absolute Encoder >

Table of Contents Operation Differentiation Singleturn / Multiturn Sampling methods Functional Safety - Motor Feedback
Subscribe to singleturn encoders