Skip to main content

Kollmorgen Support Network

Remove Safety Card - STO Bridge >

Dear community, Some problems with a safety card is stopping a machine with S700 drives from working.  We want to remove the safety card but we can not since we don't have the required "STO bridge" to detect the STO inputs. Therefore, -S- is…

S700 Safety Card S1-2 Safe Brake Control Error >

My application has a 115VAC external holding brake connected to an external relay driven by the SBC+ and SBC- output from the S700 safety card. Because the brake isn't connected directly to the safetycard, I'm getting error "Output SBC+/- does…
Subscribe to safety card