Back to top

Many customers want to use an Absolute Feedback device as the home reference.  They also want to move the axis to, what they want as, a home position and "Auto Set drive parameter FB1.OFFSET for the difference between the Absolute Feedback zero position and their pefered home position.  Attached is a RSlogix 5000 example on how to do this over EIP.  The attached zip file has a sample program and two Add-in function blocks used by the sample program.