Back to top

The PxMM can work with data from an external or shared drive. Mounting is the software process in the PxMM that enables it to read and write data to/from a shared drive. If the mounting process fails in the PxMM the following message will appear in the IDE Controller Message Log.

Shared Drive failed to mount. ExitCode: 1, Message:Network configuration: Mount the shared directory gcode to /mount/shared

One common cause in a Windows 10 operating system is that the SMB1 was disabled. To enable it:

This video introduces the KAS IDE, ST (Structured Text) Editor

Covered in the Video:

  • Syntax
  • Compile, run, and animation
  • Comments
  • Using Function and Function Blocks
  • Conditional Statements
  • Shortcut keys
  • (Reference to) Debugging

You have just received new KAS installation files consist of KAS IDE installer and PxMM Controller FW. Follow the steps below to upgrade your KAS System to the newer version.