Skip to main content

Kollmorgen Support Network

Protection Category >

The protection category is mentioned as a short mark which consists of two unvarying letters IP and ratios for the protection level. The IP codes are defined in IEC 60529. Example IP54:
Subscribe to protection class