Skip to main content

Kollmorgen Support Network

KAS ST (Stuctured Text) Editor >

This video introduces the KAS IDE, ST (Structured Text) Editor Covered in the Video: Syntax Compile, run, and animation Comments Using Function and Function Blocks Conditional Statements Shortcut keys (Reference to) Debugging

Changing variable values over Telnet to AKD BASIC program >

This application note details how to pass values via Workbench terminal, Hyper terminal, or some other method ( i.e. high level programming language, etc. ) via Telnet commands.

Programming IDC SmartDrives >

The programming language for the IDC SmartDrives is "BASIC-like", meaning that it functions like BASIC programming.  However, the language and syntax is a simplified variation of BASIC.  Each drive has either 200 or 400 programs depending…

Macro Programming >

Valid for S300, S700
Subscribe to programming