Back to top

The PDO Ethercat channel provides deterministic, fast update of parameters between the KAS controller and drives (through Ethercat). The PDO Selection Mapping tab provides an method to link PDO parameters to variables in the application code. The following example shows mapping the Drive Status word bits  to (bool) variables in the project.

The drive Status Word bit definitions are as follows:

image