Back to top

New Features

  • EtherCAT Diagnostics with:
    • Web-server tab with network topology
    • Functions/FBs for application program
    • Configurable Working Counter limit in the IDE
  • New HMIs: X2 Panel Models
  • New KVB v2.20 software
  • New function: MC_MoveVelocity(...)
  • FFLD Editor Comments
  • Ethernet/IP and Profinet Stack upgrades
  • Support for AKD v1-16, including EtherCAT RevisionNo

For more details, please see the attached release note.

KAS 2.12 introduces the following functions / function blocks which help with diagnosing EtherCAT network issues.

Below are three embedded videos showing different features of the FFLD or Free Form Ladder Diagram editor in the KAS IDE software that can be used to write PLC code.

The first video shows shows how you can organize your code into separate networks, different options to add comments to your code, and how to add the different types of contacts and coils available.

The KAS PxMM Controllers contain a built in webserver for access to the PxMM without having to work through the IDE. Functionality include:

Below is a video showing the steps to create a new PLCopen axis in the KAS IDE. First you will add an axis by right clicking the PLCopen section in the Project Explorer. After giving the new axis a name, you can open a pop-up window to modify the default axis settings. First, you can select if it is a servo axis that will be mapped to an AKD drive, a virtual axis, or a digitizing axis mapped to an external encoder. Then, you can setup the user units per rev for the axis with the ratio formed between the User Units and Drive Interface Unis parameters.

The following chart outlines the networks (field buses) supported by the PCMM and PDMM and the key  parameters of each.

image

Hardware Revision Firmware Version Date Remarks
DB 1.6 30.05.2012 Starting version, incl. AKD HWR D and PDMM HWR B
EB 1.13.0 and later 2014-12 Hardware revision for export classification traceability purposes

You have just received new KAS installation files consist of KAS IDE installer and PxMM Controller FW. Follow the steps below to upgrade your KAS System to the newer version.

Below are step by step instructions with screenshots on how to integrate a 3rd Party EtherCAT device onto a network with a PDMM or PCMM controller using KAS IDE software. There are also two embedded videos showing how to access all of these parameters in the software. The first video shows the main three steps to integrate a 3rd party device onto the EtherCAT network including importing an ESI file, scanning the network, and mapping program variables to PDO inputs and outputs.

Attached is a video demonstrating features of the PxMM web server. It can be accessed inside the IDE or directly from a web browser.

Capabilities include:

Pages