Back to top
File Description 
KAS Runtime Firmware for 1.2 GHz AKD PDMM. Note: PDMM Runtime version and KAS IDE version must be identical (e.g. both must have version 3.00.x.zzzz). This is a patch version for the initial v3.02 release.
Language 
English
Release 
3.02
Release Date 
Tuesday, July 30, 2019

The following table provides a resource for what firmware is associated with each release of the KAS IDE. This includes both firmware for the drive built into the AKD-PDMM controller, as well as the firmware for other drives that may be used within KAS.

File Description 
KAS Runtime Firmware for 800 MHz AKD PDMM. Note: PDMM Runtime version and KAS IDE version must be identical (e.g. both must have version 3.00.x.zzzz). This is a patch version for the initial v.3.01 release.
Language 
English
Release 
3.01
Release Date 
Friday, January 4, 2019
File Description 
KAS Runtime Firmware for 1.2 GHz AKD PDMM. Note: PDMM Runtime version and KAS IDE version must be identical (e.g. both must have version 3.00.x.zzzz). This is a patch version for the initial v3.01 release.
Language 
English
Release 
3.01
Release Date 
Friday, January 4, 2019
File Description 
KAS Runtime Firmware for 800 MHz AKD PDMM. Note: PDMM Runtime version and KAS IDE version must be identical (e.g. both must have version 3.00.x.zzzz).
Language 
English
Release 
3.01
Release Date 
Wednesday, January 2, 2019
File Description 
KAS Runtime Firmware for 1.2 GHz AKD PDMM. Note: PDMM Runtime version and KAS IDE version must be identical (e.g. both must have version 3.00.x.zzzz).
Language 
English
Release 
3.01
Release Date 
Wednesday, January 2, 2019

New Features

  • AKD2G Drive Integration:
    • Single and Multi-Axis drive variants
    • Firmware download
    • Digital and Analog I/O
    • Features not yet available: Capture, Feedback #2-5, Backup/Restore
    • Note: Please contact Kollmorgen for latest AKD2G firmware and KAS software.
  • PCMM Dual-Core model
    • Fully supported with PLCopen and PipeNetwork Motion Engines
  • Multiple KAS versions installed on the same computer
  • IDE Ease-of-Use Enhancements

The attached KAS projects are blank templates for users that want to start completely from scratch. They do not have sample code, control panels, and KVB projects that other template programs built into the KAS IDE software have. They only contain calls to subprograms that are available at this KDN page (https://www.kollmorgen.com/en-us/developer-network/initialize-ethercat-communication-and-motion-engine/) and will call initialization code to build any cam profiles, PLCopen axis, and Pipenetwork blocks setup in the Project Explorer of the KAS IDE software.

The following video goes through the steps needed to create a subprogram (sometimes called User Defined Function Block or UDFB), call the UDFB in another PLC program, and monitor code inside the UDFB while a project is running. This is useful for when similar or identical code needs to be called in multiple locations or for multiple axis.

File Description 
KAS Runtime Firmware for 800 MHz AKD PDMM. Note: PDMM Runtime version and KAS IDE version must be identical (e.g. both must have version 3.00.x.zzzz).
Language 
English
Release 
3.0
Release Date 
Monday, August 20, 2018

Pages